About Measurements
Keysight 89600 VSA extends the traditional one measurement-at-a-time capability to multiple measurements-at-a-time. The "Multi-Measurement" feature provides simultaneous analysis of multi-standard, multi-format, or multi-carrier signals. Each individual measurement's data acquisition and signal processing are run concurrently. All individual measurement trace data results can be shown together "side-by-side" in a combined output. To learn more about Multi-Measurements, see Multi-Measurements Overview.
Multiple Measurements
The Measurements Dialog is used to create, run, and manage multiple measurements. If you are not familiar with 89600 VSA's multi-measurement capability, review the Multi-Measurements Overview topic. This topic provides valuable information that will help you to use the 89600 VSA multi-measurement features.
Click one of the following links for more information about configuring multiple measurements.
- Multi-Measurements Overview: Learn about multi-measurements
- Analyzer Configurations: Create a new analyzer configuration
- Measurements Dialog: list all the measurements; configure hardware acquisition type and other settings
- Managing Multiple Measurements: How to add, remove, save, recall, etc.
See Also
Use Cases for Multi-Measurement
Managing Multiple Measurements
TRIG OUT Measurement example